Post Go back to editing

max40203 spice model Enable pin when used in LTspice

Category: Hardware
Product Number: MAX40203

When simulating the max40203 the subcircuit shows  a low impedance from EN to the 0 (gnd) node

quote from the model:

Ret EN EN1 300
Cet EN1 0 2.5u
Rfa EN1 0 100

this is reflected by a 9mA input current into the EN pin.

apparently simetrix does read the 0 node not globally, while ltspice does.

when is an LTspice model available ?