Post Go back to editing

ADP8140 + LT8334 Application does not provide sufficient power

Category: Hardware
Product Number: LT8334

Hey everyone,

for a LED application I am using a ADP8140 in combination with a LT8334 similar to the examples in the ADP datasheet.

In the following you can see my circuit:

There is a Voltage source of 12V and the ADP is supposed to regulate the output voltage in a range between approximately 22V and 28V to power LEDs with a maximum current of 500mA per Sink.
I built up a similar circuit with a Texas Instruments booster but i wanted to try one from AD as well.
Now the problem is:
1. The booster provides ca. 800mA maximum current befor it "cuts out" which is way below the required 4x500mA (The  inductance has a sat current of 10A)

2. There is a quite substential noise in the signal (below you can see the voltage i measured across the resistor right before the LEDs)

Is there a obvious error in my circuit? Where should i start too look to tackle these problems (I assume my ADP works fine as it does so with the other booster)?

All the best
Jordi

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.