Post Go back to editing

Parallel LTM4636

Category: Hardware

Hello, I am using the LTM4636 in a four phase configuration. The output voltage is designed to be 0.8 volts. The input voltage is 5V and I have connected INTVcc to Vin. I have also tied PVcc to Vin as directed by page 8 in the datasheet. On page 25 under the Layout Checklist/Example they have a suggestion about the COMP and VFB pins when in parallel operation.

The Checklist says to connect the COMP pins to the VFB pins when in parallel operation but that is not shown on the 4-phase example on page 31 or on the pins description page.

Can you please help me.

Thank you

Joe