ADP5074
Recommended for New Designs
The ADP5074 is a high performance dc-to-dc inverting regulator used to generate negative supply rails.
The input voltage range of 2.85 V to 15 V supports...
Datasheet
ADP5074 on Analog.com
Hello,
I have configured the ADP5074 in the circuit below for testing. However, it seems that the expected output current of 2A is not being achieved. When a load consumes more than 1A on the load side, a voltage drop of -3.3V occurs.
Q1. Is it possible to check if there is a problem on the circuit side?
Q2. If there is no issue with the circuit, could you provide guidance on which areas to debug?

Thank you