Post Go back to editing

Experiencing a high inrush current with the LT1952-1 Demo Circuit DC1317A-D.

Category: Hardware
Product Number: LT1952

Hi, 

I need help with the Demo Circuit DC1317A-D. 

I used the same schematic, but with a different transformer, which was a customized. And when I was powering it up, I found that the switching of the primary MOSFET was stopped every cycle due to very high inrush current which triggered the overcurrent protection of the IC LT1952-1. 

I was wondering whether it is caused by the transformer or there was something that I missed out in the design. 

If it was caused by the transformer, what are the specs of the transformer that I should pay attention to when I customize? 

Thank you 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.