Post Go back to editing

About MAX8216 internal resistance

Category: Hardware
Product Number: MAX8216

Hi,
I'm considering MAX8216.
When I was evaluating it, it appeared that the internal resistance was larger than 168kΩ based on the voltage at the +15V terminal.

The input resistance (5pin) is 168kΩ (typ), but what are the min and max?

A 63kΩ resistor is attached to the 5pin externally and 20.9V is applied.
If min and max are not disclosed, is there no other way but to adjust the threshold by adjusting the external resistor?

Best regards,

Yuya



tagged
[edited by: GenevaCooper at 2:52 PM (GMT -5) on 29 Jan 2024]
Parents Reply Children
No Data