Hello everyone,
I have an issue where my output voltage on the LTC3851 is being regulated incorrectly. What is happening is that the output voltage is set to 0.8 V even though It should be 5V. What is happening is that once the TK pin hits the 0.8 V mark, the output voltage drops to 0.8 V. I should note that the output voltage does ramp up to 4V before dropping to 0.8.
I have a LTSPICE simulation. Which I will post here. I slowed down the ramp voltage by placing a 2.2 uF cap on the TK pin. Other then that everything else is the same.
I have been having this issue for a while now and any assistance is greatly appreciated.
Here is my simulation file:
Here is a picture to my output voltage waveform.