Post Go back to editing

SPICE Model for MAX6495 not working

Category: Hardware
Product Number: MAX6495

Dear members

Could you please help with the following?

I imported the Spice model from the MAX6495 page into LTSpice version 17.15.

using the "Create symbol command" method.

It would seem that something is amiss with the model though.

I changed the extension from "asy" to txt only due to the upload file type restrictions.

Version 4
SymbolType BLOCK
RECTANGLE Normal -32 -56 32 56
WINDOW 0 0 -56 Bottom 2
WINDOW 3 0 56 Top 2
SYMATTR Prefix X
SYMATTR Value MAX6495
SYMATTR ModelFile C:\Projects\RSPMU\Hardware\Sim\max6495.fam
PIN -32 -32 LEFT 8
PINATTR PinName 1
PINATTR SpiceOrder 1
PIN -32 0 LEFT 8
PINATTR PinName 2
PINATTR SpiceOrder 2
PIN -32 32 LEFT 8
PINATTR PinName 3
PINATTR SpiceOrder 3
PIN 32 32 RIGHT 8
PINATTR PinName 4
PINATTR SpiceOrder 4
PIN 32 0 RIGHT 8
PINATTR PinName 5
PINATTR SpiceOrder 5
PIN 32 -32 RIGHT 8
PINATTR PinName 6
PINATTR SpiceOrder 6

Thank you

Regards