Post Go back to editing

Switch between 12-24V Power in and USB-C

Category: Hardware
Product Number: LTC4412

I want to use LTC4412 in my PCB as power switch. My Primary Power is 12-24V from Adopter and Auxilary Power is 5V from USB. In normal condition when Auxilary power is detected then system will disconnect Primary power from Load. But that's not my concern. My issue is if primary power is not available at load and then if i connect Auxilary power(USB) then will system detect the USB and power will be supplied to the system Via USB or Primary power has to be connected all the time before switching to auxilary power?

Also i will not control this IC from MCU so what should be status of other pins in hardware design?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.