Post Go back to editing

LTC3531ES6-3.3 Abnormal Input Current Drain

Hello,

I am having problem where the LTC3531-3.3 is draining more current than it is supposed to after a few months in service. My input voltage is coming from a supervisor circuit which output 5V from a DC-DC converter or 3.6V from a battery depending on which is higher.

With a brand new LTC3531-3.3 installed, the current would be a maximum of 50-100uA at 3.6V input. However, after a couple months, the same setup would drain 5-15mA instead. This is causing my battery to deplete faster.

1) What could be causing the LTC3531-3.3 to degrade like this? 

2) Does the input capacitor have to be 2.2uF or can it be higher?

thank you

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.