Post Go back to editing

Isolated power supply

Hi,

The datasheet for the DC590B states that an external power supply can be used instead of the on-board LT3439. For this, the JP5 jumper needs to be placed into the 'off' position and the supply attached to V+ and AGND. The 'Isolated Supply Options' section in the manual states that this supply needs to be between 7V and 10V. Yet, Page 1 of the manual which shows the circuit board states that the supply should be between 10-12V. Which one is correct? I suppose it's safe to use a 10V supply, but it'd be good to know what the actual parameters are.

Thanks,

Carsten

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.