Post Go back to editing

LTC3108-1

Category: Hardware
Product Number: LTC3108-1

Dear Forum members,

I was trying to boost the voltage generated with TEG. I have connected VS1 to VAUX, VS2 to VAUX. VIN and Ground to TEG. and VOUT and Ground to voltmeter to measure the voltage. However, the output voltage is less than 20mV.

In addition, I used three other connection methods:1.VS1 to Ground, VS2 to VAUX.     2.VS1 to VAUX, VS2 to Ground.      3.VS1 to Ground,VS2 to Ground.            As a result, The output voltage are also less than 20mV.

The voltage produced by teg is about 30-50mV.

How can I achieve voltage values above 3V with LTC3108?

What could be the remedy to this?

I will be happy to have your thought and advise on this.

Parents
  • qis,

    I think I know why your output voltage is near zero.  I did a retest and accidentally reversed the thermal flow, and the output was then ~20mV just like yours.  TEG modules are standardized regarding the orientation of the junctions.  One must apply the cold surface to the side of the TEG which has the identification lettering.  The hot side is the surface without lettering.

    FYI, with the test set described in my previous message with VS1=VS2=VAUX I'm getting about 4.5V when I should be getting 5V.  With VS1=GND and VS2=VAUX I'm getting 3.7V instead of 4.1V.  Either way it's about 0.5V off.  The LTC3108 system is working well enough for me to proceed.  Either the datasheet is simply wrong or there's something which isn't clear in the datasheet.  The energy conversion works, it's just grossly out of spec.

    Steve 

Reply
  • qis,

    I think I know why your output voltage is near zero.  I did a retest and accidentally reversed the thermal flow, and the output was then ~20mV just like yours.  TEG modules are standardized regarding the orientation of the junctions.  One must apply the cold surface to the side of the TEG which has the identification lettering.  The hot side is the surface without lettering.

    FYI, with the test set described in my previous message with VS1=VS2=VAUX I'm getting about 4.5V when I should be getting 5V.  With VS1=GND and VS2=VAUX I'm getting 3.7V instead of 4.1V.  Either way it's about 0.5V off.  The LTC3108 system is working well enough for me to proceed.  Either the datasheet is simply wrong or there's something which isn't clear in the datasheet.  The energy conversion works, it's just grossly out of spec.

    Steve 

Children
No Data