Post Go back to editing

LT3518 - inductor

Category: Datasheet/Specs
Product Number: LT3518

Hi,

Q1.) Based on below application circuit from the LT3518 datasheet for boost mode:

FSW 1MHz and tsw 1us

VLED 34.56V, ILED 0.3A, Ripple current = Delta.ILED=30%*ILED=0.09A

DBOOST 0.769

Calculated L= 68.31uH for VIN 8V and 95.5uH for VIN 16V

How is 8.2uH derived in the application circuit in this case?

Q2.) For a similar circuit, FSW 1MHz, Vout 16.2V, Iout 0.357A, Vin 5V, based on above formula I get, 32.26uH (for 30% ripple). 

Is this much inductance required? what would be the recommended range?

Thanks

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.