Hi,
I am using VCU118 from Xilinx. There are 4 devices of VT1697SB connected to MAX20751 for VCCINT power supply.
I used a maxim digital power tool to read the power supply.
the maxim digital power tool shows there is no input 12V coming to device and the temperature is also not read.
but I can measure 12V input going to the MAX20751 and also VT1697SB with a multimeter on board.
I want to understand why the maxim power tool is not reading the input? if it is problem with the VT1697SB devices or problem with MAX20751
Thanks