Post Go back to editing

Malfunction in ADP2443 after some years

Thread Summary

The user is experiencing issues with the ADP2443 in an SMPS design, where the IC fails to maintain a stable 3.3V output, especially when cold. The IC shows strong negative pulses on the SW output when the output voltage rises to about 4V. Replacing the IC restores proper operation. The support engineer requested the schematic diagram for further analysis.
AI Generated Content
Product Number: ADP2443

Good morning,

I have this product into our SMPS used to lower a 24V DC input down to 3.3V, 1A average load. The IC is externally clocked / synchronized to a supervisor microcontroller which also checks for the proper functioning of other supplies on the board, synchronization frequency is 606KHz.
After 3 years, I'm are getting some faulty units back and I noticed that the microcontroller starts the ADP2443 then it switches it off almost immediately because it cannot keep the output voltage properly at 3.3V, then it keep retrying indefinitely, but it cannot start correctly.

I also noticed that heating the IC makes it to function almost correctly for some time, while freezing make it to work very badly. I then bypassed the supervisor microcontroller to force the ADP2443 on and here's what I got:

Yellow trace is the SW output going to a 6.8uH inductor, the purple trace is the output voltage: the IC is not working properly at all, but the things are worsen when
freezing it slightly and here's what happens. Voltage rises up to about 4V then PWM stops then it starts again.

If the IC is replaced with a new one, correct and stable operation is restored, no matter if it is heated or frozen.

In your opinion, what could be the cause of this failure ?
When output voltage begins to rise, there are strong (-10V) negative pulses on the SW output, just like if the output mos switching to ground isn't working properly. 
Can we modify the circuit to prevent this failure in future ? Is there anything else could we check ?

Many thanks.

  • Hi,

    Kindly provide the schematic diagram of ADP2443 section.

  • Here the Electric Diagram as you request

    VBR

    Fabio

  • Hi  ,
    It would seem that this has been placed in my job jar after some years. I apologize with the lapse in ongoing assistance! I will try my best to solve your problem; I am not sure if  's scheme is also yours but unless you say otherwise I will assume so.  

    I want to start by saying thank you for the detailed write-up, the scope captures, and the schematic... all three together give us a clear picture. My assessment and recommendations are below.

    Root-cause assessment

    Everything you've described points to an internal wear-out of the low-side (synchronous rectifier) MOSFET / its gate drive inside the ADP2443, rather than a fault in your external components or supervisor:

    • A new IC restores correct operation regardless of temperature, which localizes the defect to the die.
    • Hot = better / cold = worse is the classic signature of a marginal MOSFET turn-on threshold. Vth has a negative temperature coefficient, so cooling raises the effective threshold and pushes a weakened low-side device out of full enhancement, degrading synchronous rectification.
    • The ~4 V output pump-up followed by PWM stopping and retrying is consistent with the output reaching the overvoltage-protection threshold (~121% of 3.3 V) and entering the hiccup/restart loop your supervisor observes.
    • The strong –10 V negative pulses on SW are the key clue: they indicate the low-side switch is not clamping SW to ground, so freewheel current is forced into the parasitic loop inductance.

    Critically, those repetitive negative SW excursions exceed the SW pin's negative absolute-maximum rating, and we believe they are both the present symptom and the long-term stress mechanism that degraded the parts over three years of switching.

    What we see in your schematic

    Reviewing the design, there are a few things that would drive exactly this SW-node stress:

    1. No SW-node protection. SW goes through R24 straight into L1 with no RC snubber and no negative clamp anywhere on the node. There is nothing to damp the ringing or catch the negative undershoot, so it can swing to –10 V and stress the low-side FET/SW pin every cycle. Note R24 is marked "TBD"... please confirm the value actually populated, since a series/damping resistor there would help.
    2. Thin high-frequency input decoupling. Input decoupling is 2× 10 µF (C11/C12) on the 28 V rail, but we don't see a small HF ceramic directly at the PVIN pins. At 28 V with any lead/parasitic inductance, sparse HF decoupling worsens hot-loop ringing, which feeds back into the SW undershoot. We'd recommend adding a 100 nF–1 µF ceramic right at PVIN/PGND.
    3. Free-run frequency set above the sync clock. R29 = 270 kΩ sets the internal free-running frequency to ~622 kHz, while your external sync clock is 606 kHz. It's generally preferable to set the free-run frequency below the external clock so the part locks cleanly and pulls up to it. Setting it above can produce marginal locking and frequency wander (consistent with the 615 kHz / ~920 kHz bursts in your captures). We'd suggest re-setting RT for roughly 500–550 kHz free-run and re-verifying lock.

    Recommended design changes to prevent recurrence

    1. SW snubber: Add an RC snubber from SW to PGND (start ~2.2 Ω + 1 nF, then tune to the measured ring frequency).
    2. Negative clamp: Add an external Schottky from PGND to SW (cathode on SW), rated for peak inductor current, to hold negative undershoot to ~–0.3 to –0.5 V and keep SW within absolute-maximum.
    3. Slow the high-side edge: A small series resistor (2–10 Ω) in the BST path softens high-side turn-on dv/dt and reduces the resulting undershoot (minor efficiency trade-off).
    4. Tighten the hot loop: Minimize the PVIN → high-side → low-side → PGND commutation loop and SW copper area, with low-ESL input ceramics placed directly at the PVIN/PGND pins.

    To finalize tailored guidance, could you share:

    • A good-unit SW capture at full VIN (24 V) and load, using a short ground-spring tip (not a long ground lead), so we can measure true peak negative undershoot and ring frequency and size the snubber/clamp precisely.
    • The populated value of R24, and confirmation of whether any snubber/clamp exists on the actual PCB.
    • Your layout/Gerber around the SW node, input loop, and PGND return, plus whether there's a ground plane directly under the device.
    • Input capacitor placement relative to the PVIN/PGND pins.
    • Sync details: whether 606 kHz is always present at startup, and your intended RT free-run frequency.

      If you have long solved this issue let me know and I can close this case! If you think the issue is more serious than the design reinforcements I mentioned above, let me know and I can see about having our failure analysis people take a few of the bad ICs off your hands
      Best
      Doug

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.