Post Go back to editing

LT4275 POE controller no powergood

Thread Summary

The user encountered issues with the PWRGD and LAB_TEST_OUT signals staying high on the DC2093A demo board (LT4275 and LT4321) when connected to the PSE demo board 2579A (LTC4279). After verifying connections and testing with a 50 Ohm load, the problem was resolved by ordering a new LT4275 demo board, suggesting a potential issue with the original board's MOSFET HS.
AI Generated Content
Category: Hardware
Product Number: DC2093A-A

Hi,

We are trying to use demo board DC2093A ( LT4275 and LT4321 ).

We use the PSE demo board 2579A ( LTC4279 ) for POE injection.

We connect a resistor between Vout+ and LAb_Test_Vout_-

After power ON, led on the demo board is going green. But the power good signal stay UP. Lab_Test_Pin stay to Vout.

We can see the 3 steps POE on the Vout+.
We try different configuration on both board without success .

What did we forget ?

Regards

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.