Post Go back to editing

Using a digital potentiometer like AD5175 to set the output voltage of LT3045-1

Thread Summary

The user asked if using a digital potentiometer like the AD5175 to set the output voltage of the LT3045-1 would affect its noise performance. The final answer indicates that the AD5175 should not cause the LT3045-1 to be noisy, provided the usual capacitor from the SET pin to GND is in place.
AI Generated Content

Could we use a digital potentiometer like AD5175 to set the output voltage of LT3045-1, would it effect it's noise performance?