Post Go back to editing

LT4293 Demo Board (DC2911A) LAB_TEST_VOUT- pin

Thread Summary

The user inquired about the risks of applying a resistive load directly across VOUT+ and VOUT- on the DC2911A demo board instead of using the LAB_TEST_VOUT- pin. The final answer explains that doing so can increase MOSFET stress during inrush, potentially causing component damage and non-IEEE compliant behavior. The LAB_TEST_VOUT- pin is a low-side switch that closes after inrush, simplifying evaluation with resistive loads. Capacitive loading of LAB_TEST_VOUT- should be avoided to prevent stressing Q11.
AI Generated Content
Category: Hardware
Product Number: LT4293

Hi,

I want to ask for a little more details regarding the LAB_TEST_VOUT- pin on the DC2911A demo board.  I see that it's intended for lab testing with a resistive load.  Just want to get a good understanding of what are the risks if I apply a resistive load across the VOUT+ and VOUT- instead of using the LAB_TEST_VOUT- pin?  Want to confirm if the LAB_TEST_PIN-  is to protect instances with transients when the load is shorted while PWRGD is high enabling the LT4321? So would the risk here be potentially damaging the LT4293 device and possibly the Q1 FET? 

Thanks for the help and insights.

Jerry

  • Hi Jerry,

    Due to an issue with EZ I did not receive notifications for this post. My apologies. I understand this reply is likely too late to be useful for you. In case anyone else has a similar request, I will answer your question.

    Applying a resistive load across VOUT+ to VOUT- increases hotswap MOSFET stresses during inrush up to component damage and may cause non-IEEE compliant behavior. The LT4293 controls the Q1 gate voltage to set the current flowing into C4. Any resistance at VOUT+ to VOUT- will present an additional current. LAB_TEST_VOUT- is a low-side switch that closes after inrush has completed, simplifying evaluation with resistive or uncontrolled loads. You should not capacitively load LAB_TEST_VOUT- as that would stress Q11.

    Best Regards,

    Eric