Post Go back to editing

Monitoring 3 voltages with MAX16042

Category: Hardware
Product Number: MAX16042

Hello,

I would like to use MAX16042 for monitoring 3 voltages and generating an alarm if any of the voltages is under a threshold.

The voltages I have to monitor are 5V, 12V y 24V.

I will configure the thresholds for each voltage, but I have a doubt about the Vcc voltage. Which one should I use? The highest one, 24V?

Thanks!!!

Parents Reply Children
No Data