Post Go back to editing

MAX25511 PIN 17 DIM Voltage

Category: Hardware
Product Number: MAX25511

Hi Sir,

1. What's the volatge of DIM pin if it is flaoting?

My custoemr is doing experiment. They found when they turn on the "AUTO FADE-IN/OUT" function. The DIM pin volatge is 1.5V when they do not give DIM pin power.

They are curious about the 1.5V of DIM pin is resonable or not. (By th way, I already remind, if they do not need DIM function, they should connet DIM PIN to 5V or lower. )

2. What's the lower voltage meaning of pin 17 in the pin description?  What's the rage?

Thank you~

Edit Notes

tagged
[edited by: GenevaCooper at 4:44 PM (GMT -5) on 4 Dec 2023]