Post Go back to editing

LT3045 output error

Category: Hardware
Product Number: LT3045

Hi,

 The LT3045 used in my product output abnormal.

 The 16 pieces of LT3045 was used in my product, which convert  the +4.2V to +3.3V. The 16 pieces of LT3094 was used in my product, which convert  the  -4.2V to -3.3V..  The LT3045 and LT3094 supply power to 128 pieces of AD8336. 

  1. The 11 pieces of LT3045 output -0.58V when -4.2V power was supplied first. The other 5 pieces of LT3045 was normal and output +3.3V. The voltage of “SET” pin was -0.52V. This error will continue to exist even if +4.2V has been powered on.
  2. All the 16 pieces of LT3045 output 3.3V when +4.2V power was supplied first.
  3. The 16 pieces of LT3094 is always normal。 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.