The output voltage of ADP1755 is the same as the input voltage。The input voltage of this is 2.5V, and the output is also 2.5V
ADP1755
Production
The ADP1754 / ADP1755 are CMOS, low dropout linear regulators that operate from 1.6 V to 3.6 V and provide up to 1.2A of output current. These Low Vin...
Datasheet
ADP1755 on Analog.com
The output voltage of ADP1755 is the same as the input voltage。The input voltage of this is 2.5V, and the output is also 2.5V