The output voltage of ADP1755 is the same as the input voltage。The input voltage of this is 2.5V, and the output is also 2.5V
ADP1755
Production
The ADP1754 / ADP1755 are CMOS, low dropout linear regulators that operate from 1.6 V to 3.6 V and provide up to 1.2A of output current. These Low Vin...
Datasheet
ADP1755 on Analog.com
The output voltage of ADP1755 is the same as the input voltage。The input voltage of this is 2.5V, and the output is also 2.5V
Can you share a schematic of the application?
The schematic looks fine, and the part should be regulating to 1.3V output. Is there any reason to believe there is any device damage? Does this happen on multiple units?
The schematic looks fine, and the part should be regulating to 1.3V output. Is there any reason to believe there is any device damage? Does this happen on multiple units?
hi,I have one more question,Can you help me take a look at this again