Post Go back to editing

Gate-Driver ADUM4221

Category: Hardware
Product Number: ADUM4221

Hello,

I'm inquiring about the ADUM4221 Gate Driver. I've performed a simulation in LTspice for a half-bridge power electronics application,

but I'm encountering issues where I can't effectively control the high-side MOSFET.

Do you have any example circuits or resources available for the ADUM4221 that I could reference?

My objective is to conduct the simulation without the use of a bootstrap circuit, as I require an isolated gate driver for this purpose.

Parents
  • Hi Patty,

    Thanks for your interest in using the ADuM4221. I can see that your supplies V1 and V2 are referenced to common GND which cause the issue. You should reference your V1 to GNDA (MW_O) so that your high-side FET will see the full 12V gate driver voltage. Same as with V2, the ground connection should be connected to GNDB or MW_U.

    I'm not sure if your are aware of this, but there we example of basic circuit of each of the part if you navigate to your LTspice folder --> example --> Applications as shown below.

    Let me know if you require further assistance.

    Best regards,

    Jefferson

  • Dear Jefferson,

    I want to express my gratitude for your prompt response and the valuable recommendation you provided. I made adjustments to my LTspice circuit, and the simulation now functions significantly better. This has enabled me to successfully control the high-side MOSFET.

    I also managed to locate example circuits within the data path, but I am currently using the Gate-Driver as depicted in the attached images.

    However I am using the Gate-Driver in the following as shown in the pictures: 

    However, I noticed in the datasheet for the ADUM4221, they illustrate a bootstrap circuit. Is this bootstrap circuit necessary for controlling the high-side MOSFETs, or can I achieve the same control of the half-bridges as shown in my LTspice circuit?


    I've included the datasheet circuit for your reference. My ultimate goal is to control a full-bridge circuit composed of these half-bridges.

    Thank you once again for your assistance.

    Sincerly,
    Tahir 

  • Hello Tahir,

    Great to read that your circuit is already working. Just take note of the GNDx connections in your actual implementations. Slight smile

    For the bootstrap recommendation - it is just a recommendation if you like to power the secondary side of the gate driver with a single power supply (VDDB from Figure 38). 

    However, if you have means to provide an isolated power supplies for the high-side gate drivers separately - this is absolutely okay (same as with the LTspice circuit you provided).

    Let me know other concerns you have and I'm happy to help.

    Best regards,

    Jefferson

Reply
  • Hello Tahir,

    Great to read that your circuit is already working. Just take note of the GNDx connections in your actual implementations. Slight smile

    For the bootstrap recommendation - it is just a recommendation if you like to power the secondary side of the gate driver with a single power supply (VDDB from Figure 38). 

    However, if you have means to provide an isolated power supplies for the high-side gate drivers separately - this is absolutely okay (same as with the LTspice circuit you provided).

    Let me know other concerns you have and I'm happy to help.

    Best regards,

    Jefferson

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.