Post Go back to editing

Need suitable part to generate 3.3 V (at least 750mA) from an input between 3-12 V. Device needs to run from both single Li-Ion cell, as well as 12V

Category: Hardware

I've been looking at datasheets for a while, and nothing jumps out as clearly suitable.

Two possibilities are the LT3467, and the LT1930? Would those work?

Edit Notes

Added detail
[edited by: jaxeuelpw at 7:25 PM (GMT -4) on 5 Oct 2023]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.