Post Go back to editing

the SYNC pin on the LTM8033

Category: Datasheet/Specs
Product Number: LTM8033

When not using the SYNC pin on the LTM8033 and disabling burst mode, the data sheet states, "Connect the SYNC pin to a stable voltage greater than 0.7V. Do not let the SYNC pin float." It is written. (8 pages, 14 pages)
Previously, it was connected directly to the power supply terminal, but since the absolute maximum rating of the SYNC terminal is 30V (page 2), we are thinking of applying a power supply voltage of 18 to 36V, so connecting directly to the power supply is not recommended. I think it's difficult.

Is it okay to connect the 36V power supply by dividing it with a resistor?
Also, the inflow current to this pin is 0.1uAtyp when SYNC=0V, but how much current should be expected when supplying it to the SYNC pin when applying an H voltage as described above? Or?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.