Post Go back to editing

LT8316 UVLO

Category: Hardware
Product Number: LT8316

Hello,

I have used the LT8316 in several of my designs. However, in my current design, I need a precise UVLO. The input voltage to my design is 350VDC and I need it to start at 300 ±10 VDC. Using LTspice or calculating the 1.22V using a voltage divider has not produced any repeatable or accurate data. The datasheet is not very informative on how the UVLO works on this chip. I'm trying to stay away from using any kind inhibit as using the UVLO could save component count.

Please help. Thanks