Post Go back to editing

LTC3880 with DC1709A with LTpowerplay does not output voltage on telemetry

Category: Hardware
Product Number: LTC3880
Software Version: LTpowerPlay

Hello, 

Im trying to have my LTC3880 output  1v to the READ_VOUT telemetry using LTpowerplay for some reason the output stays at zero no matter what.

The Input voltage READ_IN is at 4.2443 V.

I am also using the 01_datasheet_defaults.proj project file the regulator comes with.

Im simply just putting a stock LTC3880UJ into the stock Demo circuit 1709A and firing up LTpowerplay it displays everything fine but its like the device wont turn on its VOUT . 

When I go to the Simple mode GUI it shows U1:0 and U1:1 in a red color and not the green like the QuiStart Video. 

Please help on how to configure the Vout put to on. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.