Post Go back to editing

Feedback loop for LT1248

Category: Hardware
Product Number: LT1248

Hi,

I have just calculated the current feedback loop for the LT1248 Average current mode PFC controller, for a 150W PFC.

I followed the equations on page 7 to 8 of the LT1509 datasheet. When I conform to their equations, the mains input waveform is a very poor sinusoid. Then, when I just tweak the current error amp compensation components, then I can get a great sinusoidal mains input current…however, the values I use for that  are values that fail the requirements of the LT1509 datasheet calculations

Can you say whats going on with the  current error amplifier compensation equations on page 7 and 8 of of he LT1509 datasheet? Why do they give  compensation R and C values , which basically, do not work?

 LT1509

www.analog.com/.../lt1509.pdf

 LT1248SCHEM__LT1248 PFC 150W_240VAC_MyHash_greatPFC.ascSCHEM__LT1248 PFC 150W_240VAC_VoutGood_IinLookstRIANGLE.asc

www.analog.com/.../lt1248.html

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.