Post Go back to editing

MIL-STD-1275E surge stopper with input range 7-36V & output 36V.

Category: Hardware
Product Number: LT4363 LTC4366

Hi,

I require a MIL-STD-1275E surge stopper with input range 7-36V & output 36V. This will be conencted into a MAX25240 to regulate final output to 12V 2-3A as it is very efficient.

My circuit needs to continually operate during input distortions.

Reviewed:

www.analog.com/.../high-voltage-surge-stoppers-ease-mil-std-1275d-compliance.html

DN534

These solutions similar to what I need for my power input section BUT:

1. I'd like to replace the Reverse Polarity diode D1 with the solution in LTC4366 datasheet Figure 8. Is this a workable change?

2. Operate 7-36V nominally

3. Output 36V maximum. - Can I simply adjust the FB resistors?

4. Should I be looking at the LTC7860 instead?

Edit Notes

rewording 1st line to be clearer
[edited by: PaulCarson at 7:58 AM (GMT -4) on 4 Sep 2023]
Parents Reply Children
No Data