MAX25608
Recommended for New Designs
The MAX25608/MAX25608B/MAX25608C/MAX25608E/ MAX25608F 12-switch matrix manager ICs for automotive lighting applications include a 12-switch array for bypassing...
Datasheet
MAX25608 on Analog.com
Hii,
I want to use this part MAX25608 on a application.
I need to create the CRC3 for the read and the write translation. Both transactions have different number of bits as data to calculate the CRC3 as described on the datassheet.
Do someone have any code example on how to calculate the CRC3 as described on datasheet for read and write transactions?
They use pol x3+x+1 and initial value 000.
Thanks,
Eduardo
On my application I'm using 200ohm on RADDR pin and RGRADE pin to GND.
I'm sending a READ command to address 0x00, this give those bytes:
0x79 0x03 0x00 0xE0
I calculated the CRC3 bases on algorithm I found here:
MAX25608 CRC Calculation : r/embedded (reddit.com)
Is something wrong on the bytes I'm sending?
Thanks,
Eduardo.
Hi, Thank you for your inquiry. Currently, only Maxim ATE products are supported on EngineerZone at this time. Over the next several months, you will see more Maxim products being supported in EngineerZone. Please visit one of the technical support pages on our newly integrated website below for assistance with Maxim Integrated products.
EN - https://www.analog.com/en/support/technical-support.html#
CN - https://support.analog.com/zh-CN/technical-support/
JP - https://support.analog.com/ja-JP/technical-support/