Post Go back to editing

LTC3705 - Overcurrent Threshold on the "IS" pin.

Category: Hardware
Product Number: LTC3705

Hello, ADI team.

The data sheet specifies that the Overcurrent voltage threshold Vis(max) = 300mV.

My question is: What is the tolerance to narrow pulses on the "IS" waveform e.g. noise spikes that can easily be much higher than 300mV?

I can't find any such information in the data sheet.

For example, see the screenshot of the "IS" pin below. The peak "steady-state" voltage of the waveform is approx. 142mV. But look at the noise spikes at the start of the falling edge. If they were more than 300mV, what would be the maximum width that these spikes could be without triggering the OverCurrent fault condition?

Thanks.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.