Post Go back to editing

The Max17271 has the inductor Peak Current Limit and the Max77675 has the inductor Valley Current

Thread Summary

The user inquires about setting the inductor current for the MAX77675, which uses valley current control, unlike the MAX17271. The final answer clarifies that the inductor current cannot be directly configured but suggests using the spreadsheet to compute the current based on system voltage and load. Additionally, the power mode and status/interrupt bits can be configured and monitored to manage system overload conditions.
AI Generated Content
Category: Hardware
Product Number: Max17271 and Max77675
Software Version: .

The Max17271 allows to select 4 different values (register map) of the Inductor Peak Current Limit (ilim), but the Max77675 has a different approach (Valley Current), why? and how Could I set (using the register map) a specific level of the inductor current for this part (Max77675) ?

Please, could you help me?

Regards!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.