Post Go back to editing

Lt8636 Input Capacitor short to GND after a while and randomly

Category: Hardware
Product Number: LT8636
We have used LT8636 at our board as step down , the input is about 28 v and the output is about 12V and the current consumption is about 1A , now we have a problem and is that randomly the input capacitor of the LT8636 Short to GND , At the First Schematic we have only two 10uF Capacitors and the problem occurred , based on the Input Capacitor of the Datasheet we add an Electrolyte Capacitors and the problem occurred 
again , is it possible that help me to solve it please ? 
  ,

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.