Hello! I have display backlight driver made up with MAX25510 IC in SEPIC configuration. The IC does not start up above certain value of input voltage.
The circuit is as follow. The PWM DIM input is at 200 Hz, and AIM is at 0V. Load is 4 parallel strings with 6 LED in series 480 mA of total current.

If input voltage is within ~21.5 V I can see successful start and operation. The startup process is shown in next picture. The yellow chanel is BSTMON input, and green is OUT_1 input. DC-DC rumped up to OUT_ regulation (19.6 V) and IC is operational in all designed ranges of input voltage (even if I rise it above 21.5V)