Hi,
I'm experimenting with the ADP197 evaluation board.
I have two questions, please let me know.
1.
I am experimenting with the following circuit and measurement method.
Measurement procedure order
(1) Turn on the 2.2A electronic load in ②.
(2) Turn on 1.8V from the power supply of ①
(3) Get the waveforms of Vin, Vout, Iin, and Iout at this time
Chattering occurs at 1.8V, which is the very limit of the input rating.
Is this normal?
Or do you have any suggestions for improvement?



2.
I did the same experiment (2.2A with electronic load) with Vin at 2.8V.
Then, the inrush current became about 7A, and the IC was damaged.
Regarding the current, there is a description of ±4A in continuous operation,
Are there any peak absolute maximum ratings?
If you know the characteristics of the built-in FET, please let me know.
Best Regards,
Naohisa