Hello,
I have one simple question about the output voltage range of the LTC3896.
In the below datasheet, LTC3896 have lower limit of -60V.
And also, we can find the AMR(65V) of the GND pin.
Q1) Is the lower limit of -60V related to the AMR(65V) of the GND pin?
Q2) In the LTspice simulation, we can see the -80V output result like below. Then can we use this case?
Thanks in advance,