Hello,
What are the allowable values regarding overshoot and undershoot of SW waveform?
Please reply as it is not stated in the maximum ratings.
Regards,
Kazu
LT3693
Production
The LT3693 is an adjustable frequency (200kHz to 2.4MHz) monolithic buck switching regulator that accepts input voltages up to 36V. A high efficiency 95mO...
Datasheet
LT3693 on Analog.com
Hello,
What are the allowable values regarding overshoot and undershoot of SW waveform?
Please reply as it is not stated in the maximum ratings.
Regards,
Kazu
Hi Kazu,
Thanks for application of LT3963.
It seems that the max voltage rating of SW should be the same as the Vin pin, which is 36V.
Best regards,
Andrew