Post Go back to editing

MAX17262 battery capacity and current handling

Category: Datasheet/Specs
Product Number: MAX17262

I am considering using the MAX17262R for an upcoming project and have some questions about the battery capacity and current handling...

• On page 15, the maximum value represented by the capacity register is 16383.5mAh. Elsewhere in the document it is stated that "the IC provides best performance for batteries with 30mAhr to 6Ahr capacity". I am intending on using this fuel gauge with a 1S3P 3.7 battery which range from 6600mAh to 9000mAh. Is there any description or graph explaining how performance degrades for capacities beyond the 6000mAh 'best performance'?

• Since this battery fuel gauge is in the power path, I'd like to know the limits of how much current it can handle. My battery charger supports 3.5A charging, but I am concerned that one BGA pin would not handle this well. Is there any specification for current handling of this IC?

Thank you.

  • Reading the datasheet closer, there is some discussion about this on page 22 "Current Limit Based on Utilization Patterns"

    I don't understand it completely, but it seems to be expressed as percentage of the 100,000 hour lifetime of the IC.

    If I am reading this correctly, the MAX17262 can handle 1.7A continuously throughout its lifetime.

    It can handle 3.1A for 1% of its 100,000 hour lifetime (1000 hours)

    "utilization current" I assume is current from the battery to the system (as opposed to charge current)?

    I do not understand what the chart means by "10% duty.

    Anyway, it seems 1.7A is the 'safe' limit, but it's ok to go over this up to around 3A for short periods, but not continuously.

  • I think for my case, since I'm using relatively large capacity batteries, higher currents, and long-system run time (6 hours charge, 10 hours use at around 1.5-2A), I would prefer a voltage-only model-gauge, but unfortunately the current offerings from Maxim are only the MAX17058 and MAX17048, which only work with 3.7V Lithium-Ion batteries (not 3.2V LiFePO4).

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.