LTC3260
Recommended for New Designs
The LTC3260 is a low noise dual polarity output power supply that includes an inverting charge pump with both positive and negative LDO regulators. The...
Datasheet
LTC3260 on Analog.com
Hi,
I'm trying to model LTC3260 for potential use as a low noise bipolar supply for op amps in a microphone circuit (converting from single rail from phantom power found in mixers/audio interfaces/etc.). I keep getting errors or LTspice just takes forever to no avail when I run simulation. The LTC3260 is configured to regulate down to +/- 10V. Can someone tell me what I'm doing wrong here? Also are there simpler or alternative solutions to providing a clean bipolar supply from a single rail? Thanks in advance for any pointers.

Or do you think a simple mid-supply virtual ground (resistor divider) is more than enough for the ADA4075 signal buffers? Am I overthinking this?
Hello,
I did not see the ADA4075 op-amp in LTSpice but I did notice that there are many other op-amps like the ADA4077. Can a similar op-close be to simulate the LTC3260 with the op-amp intended to use?
I downloaded the official spice model from Analog for the ADA4075 since it isn't natively included in LTspice library. Frankly I'm not sure why you don't natively support a lot of your chips in LTspice. Anyhow, the whole point was to model the system in its entirety. ADA4075 is significantly quieter (which is extremely desirable in this applicaition) than ADA4077 and the quiescent requirements differ a bit. Anyhow I could give your suggestion a shot.