Hello,
My circuit is that RUN1 is connected to SN74LVC8T245 through 0Ω resistor and is pulled up to 3.3V through 10KΩ resistor. To output 1.8Vout, On signal (3.3V) is applied to SN74LVC.

<Problem>
In the above RUN drive circuit, there are some PCBs that do not output 1.8Vout. When checking the voltage, I found that RUN1=L. Pin 20 of SN74LVC is input high, but pin 4 output low.
<Verification Results>
(1) When R285 is removed and RUN1 is set to 3.3V pull-up only, RUN1=H and 1.8V output is observed, confirming normal operation.
(2) Remove R260 and operate with R285=0Ω, RUN1=L and no 1.8V output.
(3) Remove R260 and R285=0Ω was changed to 1.1KΩ, RUN1=H and 1.8V output was observed (Below circuit)

<Questions>
1: Why does the RUN1 pin go low in the state shown in Figure 1?
2: In the circuit shown in Figure 2, 1.8V is output, but I am not sure if it is appropriate as a drive circuit. To check if it is appropriate, please tell me what kind of circuit RUN1 is inside LTM4671.
Best Regards,
Kazu