Hello:
The MAX38904A datasheet table 1, in this table use "IN", " Hi-Z","GND" control sel A & sel Beq
Among them, "IN" stands for Vin? Can this input use digital I/O logic input?
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
MAX38904A
Production
The MAX38904 is a 1.7V–5.5V VIN, low-noise linear regulator that delivers up to 2A of output current with only 5.1µVRMS of output noise from 10Hz to...
Datasheet
MAX38904A on Analog.com
Hello:
The MAX38904A datasheet table 1, in this table use "IN", " Hi-Z","GND" control sel A & sel Beq
Among them, "IN" stands for Vin? Can this input use digital I/O logic input?