LT8471
Recommended for New Designs
The LT8471 is a dual PWM DC/DC converter containing two internal 2A, 50V switches and an additional 500mA switch to facilitate step-down and inverting...
Datasheet
LT8471 on Analog.com
LTC6269-10
Recommended for New Designs
The LTC6268-10/LTC6269-10 is a single/dual 4GHz FET-input operational amplifier with extremely low input bias current and low input capacitance. It also...
Datasheet
LTC6269-10 on Analog.com
Hi,
I have a power rail requirement of below
| Polarity | Voltage | Load Current | |
| + | 2.5 | 400 | mA |
| - | 2.5 | 400 | mA |
| + | 5 | 620 | mA |
| - | 5 | 330 | mA |
In my current design i depend on LT8471 where i use a 12V input to multi rail buck converter, the converter output is filtered through a CLC filter, with combinations of 0.1uF,4.7uF,0.01uF,47uF
the output then taken to a LDO again the LDO output is maintained with a CLC filter
But still my output is noisy like below
-2.5 Rail

-5V Rail

a wide snap of -2.5v rail

similar nature with the positive rails also
Effective the noise is arround 100mV Peak to peak
i have a amplifier signal chain to which this creates serious problem and i am unable to reduce the reference voltage of A/D conversion due to this problem
Below is my signal chain LTC6269-10 Followed by LNA Followed by LT6754

Kindly suggest a power solution for noise sensitive applications like FSO,LIDAR etc.
the output then taken to a LDO again the LDO output is maintained with a CLC filter
Hi,
it is not a good idea to use an CLC-Filter at the output of a LDO.
I suppose that your noise on the power rails comes from ground noise, that is generated from your LT8471 DC/DC.
Try to locate your noise source. But be aware that with a scope you can get fooled and see ghost signals, because of ground bounce.
(You can check that by connecting the crocodile clip to circuit ground and the probe tip directly to the crocodile clip.
Any signal you still see, ist from ground HF-noise)
A superior layout is absolute mandatory. for the layout, look at the demo board.
Additionally:
I would suggest that you insert ferrite beads + Cs: Converter ground to board ground and pos. and neg. rail.
Pay attention to the frequency of your noise. Choose a ferrite bead that has high impedance in that frequency region.
Be aware, that inductors have a self resonance frequency. When noise frequency comes close to that frequency it doesn't filter anymore.
Also the CLC-filter has its own resonance frequency, that should be damped ore avoided.
Better choose a ultra low noise, high PSSR LDO like LT3042 (positive) and LT3093 (negative). For your load current you would have to parallel two of it.
Or you look for stronger LDOs.
These regulators have high PSSR even at high frequencies. That eases the filter cutoff-frequency in front of it.
And they have so low noise, that an output filter will not improve that significantly .
Probably you'll better choose a C - ferrite bead - C filter in front of LDOs. Because they are better for filtering up to high frequencies.
You must choose a part with sufficient current handling.
LDOs are ok, but what about a 12V to lower voltage conversion bucks / DCDC ?
i currently use a C 10uH C filter bank, i need to try measuring noise as you said.