Hi,
I have an issue with the LTC3630. I am supplying the regulator with 30VDC and the output should be +15VDC. VPRG1 is connected to SS and VPRG2 to GND, therefore VFB is set to 5V. With the external divider R1 = 200k and R2 = 100k the output should be 15V. But unfortunately the output is always about 10.2VDC. Current draw is around 30mA.
Here the schematic:

Any clues, why the 15V are never achieved.
Thanks in advance!
Christian