LT8490
Recommended for New Designs
The LT8490 is a buck-boost switching regulator battery charger that implements a constant-current constantvoltage (CCCV) charging profile used for most...
Datasheet
LT8490 on Analog.com
LT8705
Production
The LT8705 is a high performance buck-boost switching regulator controller that operates from input voltages above, below or equal to the output voltage...
Datasheet
LT8705 on Analog.com
Hello, I apologize for my long winded nature. I tend to be explorative during my board tuning sessions which makes me find nuances with devices. So here is a lot of background:
I have two mosfets in parallel for both high and low side switching, M1, M2, M3, and M4 in my 30A LT8490 charge controller system. System functions fine but I am tuning it and was inspecting my gate driver traces and got concerned about gate driver peak current. These are some hefty gates,
The gate capacity total for both mosfets is about 6.6nF, or about 50nC.
These gate traces are 20mil, 1oz copper. They are rated I believe for 1.5A with those specs? The switch node traces are also 20mil, that is important because those
My switching frequency is 151kHz and I measure my low side switch turn on and off around 20ns and my high side about 80ns. The 8490 is rated for 20 and so are my mosfets. So the high sides are switching a bit slow but totally acceptable at 80ns.
Following some simple equations: with t being rise time, not the period . Again, simple, not getting into miller effects or adding the capacitance of the copper regions and components and snubbers.
I = C * dV/dt , inputting the data above I get roughly the following data for the various mosfets':
low side M2 and M3: 2A peak current for dV of 6.35V on the gate, 20ns, 6.6nF
high side M1 and M4: 16.5A for 50V gate, 20ns, 6.6nF
M1 and M4 experience 80ns slew, not 20ns. Which makes sense if my traces are not able to handle 16.5A, they instead saturate (or dubbed inductive impedance if I am not mistaken) and limit the current until the gate is charged enough to not draw current that saturates the lines anymore; limited gate charge up.
So I thought to widen my traces a bit to permit such amps...
So, my question is, what is the peak current limit of the LT8490 / 8705 gate drivers? Should I leave it limited like this so its safe for the driver? It functions fine, and the 8490 IC does not get warm or hot, but I hesitated and wanted to ask before I widen my traces where I may find the driver pop under the 16.5A peak.
Before you might say, "nah its probably fine where you have it, go ahead", this becomes more important as I will be powering a motor at 75V with the 8705 (same as 8490 just without the solar brains). At 75V out, that gate will reach 81V (which 8705 is rated to reach for the gate drivers), making that mosfet gate peak current reach 26.4A for my mosfets. Must I limit it which will give me a slew rate >100ns to keep the peak down?
One thing to maybe consider is the gate resistance, which I have no clarity on the internet whether that resistance is always 'active' or if thats after some inrush moment (0ohms at t=0, then reaches gate resistance when lightly charged... I do not know). My gate resistance is 2.2Ohms. This would limit any current to about 2.5A @ 6v, and 22A @ 50V and 37A @ 81V. These resistance inrush current limits are higher than what the capacitance inrush currents will theoretically draw, so maybe gate resistance for my case is not relevant.
By the way, the average current at my switching frequency (which is the low end of what this device can do) is about 3mA for the low side to 6mA high side @ 50V, 12mA high side @ 81V gate. That seems low to me, or is that a lot for this gate driver? The gate driver is powered by INTVCC which is rated for about 100mA @ 6.35V. Doing some power conversion of V * I = V * I, solving for I gate driver with 50V for example, is 12.7mA. Adding the average gate currents during buck-boost switching all 4 switches, (8 mosfets), that gives an average current of 3+3+6+6 = 18mA. My INTVCC doesnt droop; the data sheet says INTVCC has a range of 90mA to 165mA. The 165mA provides up to 21mA average current limit to the sum of all my drivers... curious? The chip again does not get hot or warm.
I did experience difficulty with some buck-boost instability, shoot through in this system and it just begs the question if this is related? Either way writing all this makes me want to double my INTVCC caps. I'll do that anyways, feels wise even if its not related.
The only information I see for driver limits in the data sheets are ratings like, 3300pF gate capacitance provides 20ns rise and fall times with some dead time values in the 200ns range. I am double that capacitance but still get 20ns on my low sides. That's the only reference I have for 'limits'.
Thanks!