Post Go back to editing

LTC4364 Over voltage cut off not working

Thread Summary

The user inquired about the overvoltage cut-off functionality of the LTC4364, which was not working as expected. The support engineer clarified that the overvoltage cut-off only activates during initial power-up if the OV pin voltage exceeds 1.25V before the 100μs power-on-reset. For continuous overvoltage protection, the FB pin must be connected and configured, as shown in the datasheet.
AI Generated Content
Category: Hardware
Product Number: LTC4364HMS-2#PBF

Hi Team,

We have designed LTC4364 for circuit for under and over voltage protection, this design the under voltage cut off functionality was working properly, but the Over voltage cut off  functionality Not.

We have set the over voltage cut off at 40V, anyone please answer why this feature not working.

Our Schematics attached below please review the same and share the feedback.

Regards,

Ajnas C

Parents
  • If we are given a 42V directly, we get 0V output, but if we slowly increase the voltage from below the cutoff to above the cutoff voltage, the LTC4364 output does get input voltage. I don't understand why the LTC4364 doesn't cut the voltage when it exceeds the limit.

    Initially when the voltage is higher than the limit, the output is 0V, and the voltage is slowly reduced, the limit goes below the cutoff voltage and the LTC4364's output shows high. When the voltage exceeds the limit, how will it be cut?

  • Hello Ajnas,

    your observations are exactly the expected behaviour. The OV-Input keeps the FET off, if an overvoltage ist detected at startup (during the first 100µs). If the input voltage exceeds the limit later, the FET will not be switched off.

    The datasheet says:

    "At power-up, if the OV pin voltage is higher than its 1.25V
    threshold before the
    100μs internal power-on-reset expires,
    .....

    the HGATE pin will be held low until the OV pin volt-
    age drops below its threshold.

    .....

    Once the HGATE pin begins pulling high, an input over-
    voltage condition detected by OV will not turn off the pass

    device.
    "

    So once the FET is turned on, it will not be turned off by an overvoltage detected at OV. In that case, the reaction to the overvoltage has to come over the FB-pin (which is not used in your circuit).

    best regards

    Achim

  • Hi Team,

    Is any IC available for the under and over voltage cut off, could you please suggest any  AEC-Q100 qualified IC with this specification?

Reply Children