Post Go back to editing

Question about replacement of LTC1966 to LTC1967

Category: Hardware
Product Number: LTC1967

Hi,

Regarding the replacement, the Vss pin of the LTC1966 becomes the NC pin of the LTC1967.

Since -5V is connected to the Vss pin, simply replacing it will connect -5V to the NC pin. Is this a problem?

Regards,

Kazu

Parents
  • Hi Kazu:  pin 4 on the LTC1967 is not internally connected, so yes you can leave it connected to -5V.  Keep in mind that the inputs of the LTC1967 in this condition will only be valid between 0V and Vcc.  Don't put a negative voltage on the inputs of LTC1967, like you can with LTC1966 on +/-5V supplies. 

Reply
  • Hi Kazu:  pin 4 on the LTC1967 is not internally connected, so yes you can leave it connected to -5V.  Keep in mind that the inputs of the LTC1967 in this condition will only be valid between 0V and Vcc.  Don't put a negative voltage on the inputs of LTC1967, like you can with LTC1966 on +/-5V supplies. 

Children
No Data