HI!
I made power board based on LTM4630 demo,As shown in the circuit below

INPUT:5-12V
But after power-on, there is no output at all;RUN1, RUN2, INTVCC, PIN voltage is normal; The CLK clock is normal.why?
Thanks!
LTM4630
Recommended for New Designs
The LTM4630 is a dual 18A or single 36A output switching mode step-down DC/DC μModule® (power module) regulator. Included in the package are the switching...
Datasheet
LTM4630 on Analog.com
HI!
I made power board based on LTM4630 demo,As shown in the circuit below

INPUT:5-12V
But after power-on, there is no output at all;RUN1, RUN2, INTVCC, PIN voltage is normal; The CLK clock is normal.why?
Thanks!