Hi,
I would like to use the LT3439 to create an isolated DC-DC converter with 5V input and bipolar output.
I need a very low ripple voltage so my idea is to connect at the output of LT3439 an LT3042 and LT3093.
I need a voltage +2.5V - 300mA / -2.5V - 300mA
Please can you susggest to me suitable diodes and the transforme for my application?
My device is power safety so I would like to realize a voltage at the output of LT3439 enough for the dropout.
Thanks in advance for your help.
Regards,
Carmelo