Post Go back to editing

LT3439 Design

Category: Hardware
Product Number: LT3439

Hi,

I would like to use the LT3439 to create an isolated DC-DC converter with 5V input and bipolar output.

I need a very low ripple voltage so my idea is to connect at the output of LT3439 an LT3042 and LT3093.

I need a voltage +2.5V - 300mA / -2.5V - 300mA 

Please can you susggest to me suitable diodes and the transforme for my application?

My device is power safety so I would like to realize a voltage at the output of LT3439 enough for the dropout. 

Thanks in advance for your help.

Regards,
Carmelo

Parents Reply Children